How to choose Rc and Cc of the BQ76930 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to choose Rc and Cc of the BQ76930 ?
R can be sized to to dissipate the extra power loss seen during the cell balancing. Also for bq76930 , the input filters -resistor Rc to keep the balance current small. Cc cap for improved measurement.
Rc is typically ( 1K) selected based on the balancing current, [ 2 *4.25/ 2 *1K ] =4.25mA. balancing current is low..but may be acceptable for expected balancing windows and overnight charging.
Also the max power per balancing resistor (4.25mA*4.25mA) *1k = 18mW
RC filter for high frequency filtering, LPF = 1 / ( 2*pi* 1K *0.1u) =1.6KHz
yes. A higher Balance current can be achieved by reducing the Rc. The power filter ( filter for the VCnX pins)
also must be reduced. The EVM schematics on the d/s use larger input Rc to reduce transient voltages to the inputs.