With the standard BQ24610 application, there are two back-to-back P-CH MOSFETs in the front end of the charger IC for over-voltage and reverse input protection. I am just wondering if these two MOSFETs can also be used for over-current protection?
For example, I have set the maximum input current via ACSET to 3.5A and the fast charging current is set to 3A. The input current sensing resistor is 0.01R. If for some reason, my system circuit tries to draw 5A current AND AC adaptor can provide this much current, will BQ24610 turn off its input via ACDDRV? Or it will just let the system draws 5A current as long as the voltage at its input is stable.