Hi, I intend to use the LDO TPS767D301QPWPRQ1 for powering a microcontroller board based about TMS320F28335 microcontroller. I observed in the datasheet that output capacitor ESR of 0.06 to 1 ohm is needed for stability for 22uF output capacitor.
I have used a 22uF ceramic capacitor as output capacitor C1 and a 0.068 ohm resistor R1 to emulate the ESR. Then, I have another capacitor C2 of 10uF connected across the output voltage, with no ESR. I have used a 0.25W resistor for emulating the ESR. Here are my questions:
1. Is the ESR resistor necessary to be a thin film resistor, or can I use a precision thick film resistor, something like the following?
The above resistor is in 0402 package, while thin film resistors are in 0603 package for 0.25W. I will be using this for automotive application, for which the said resistor rated.
2. PCB layout question: Can this ESR be on the bottom side of the pcb, while the output capacitor is on the top side? OR does this resistor have to be on the top side too?
3. Is the arrangement of C1+R1 and C2 a good one, or should I insert an ESR in series with C2 as well?
Please advise.