This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq76940 disable CHG output on SCD or OCD

Other Parts Discussed in Thread: BQ76940, BQ78350-R1

Hello,

Is it possible to configure the bq76940 to disable both the CHG and DSG outputs on a short circuit or overload condition?  

From the datasheet it looks like it can only be configured to disable the DSG output, but the bq78350-R1 user guide says it can configure it to turn off both (Section 3.1.4 of the bq78350-R1 user guide, bit setting [DC_CHG_OFF]).  I'm not using the bq78350-R1 as my host controller, but if it can configure the AFE to function in this way, can I do the same with my host controller?

Thanks,

Jess