This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22678

Other Parts Discussed in Thread: LM22678, LM22677

I used the webench designer for LM22678 and the pin connections on webench differ from that on the data sheet. I attempted to use it based on the data sheet, however, that does not appear to work (all 5 samples fried) and I'm wondering if webench is the correct pinout. Could someone verify which is the correct pinout?

One of the major discrepancies is that the input of the datasheet pinout is the output pin of the webench pinout.

Specifically, I used the LM22678QTJE-5.0/NOPB chip.

Thanks,

Trevor