My query is reg the TPS54360 ; its Thermal Resistance . The Data Sheet mentions it as 42.0*C/W for Std Board ; while Webench takes is as ICTheta JA Effective as 26DegC/W . Which is correct ? Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The 26 C/W comes from measurements on the EVM in open air. We decided to use this value because typically if we use the JEDEC standard coupon value it is very pessimistic when compared to the real performance. The thermal simulation will match this value much better if you change the edges of the PCB from insulated to open air 30 deg C. The TJA decreases to 31.7 deg C/W.
However like John said performance depends greatly on the actual PCB design and ambient conditions in the application.
Thanks to Anthony and John for the quick response.
Does that ( lower R-theta ) hold for other similar devices like LMR14020 ?
Rgds