Hello Team,
I'm having troubles starting up a battery pack protection circuit based on bq78z100 so I have a few questions about it. My circuit is very similar to the evaluation module ( bq78z100EVM ) with a 2-series cells setting.
1. Is it mandatory some kind of programming or configuration before using it?
2. Must the bq78z100 detect a voltage at PACK pin to turn on the FETs?
3. What are the conditions to turn on the FETs?
4. Does the switch (S1) have to be included in a definitive circuit?
Thanks in advance,
Jose