My LCD has two 100mA LED strings. Can I tie Outs 1 & 2 together and tie Outs 3 & 4 together to provide 2 100mA outputs on the LP8551. If not, is there a better driver to use for this application.
Thanks
Chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My LCD has two 100mA LED strings. Can I tie Outs 1 & 2 together and tie Outs 3 & 4 together to provide 2 100mA outputs on the LP8551. If not, is there a better driver to use for this application.
Thanks
Chris
Hello,
Yes it is possible to connect outputs together to get higher output current. However I would suggest connecting 1&3 and 2&4 together to optimize the output phase shifting in this case.
Thanks.
Best Regards,
Tomi Koskela