This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Documentation BQ78350 seems to be incorrect

Other Parts Discussed in Thread: BQ78350, EV2400, BQ78350-R1

Hello,

Currently I am working on a project involving the BQ78350. I need to read the SMBus with a Microcontroller, which is partially working.

I encountered some errors in the documentation that I'd like to show you. Maybe you have a solution for me.

- Lifetime Data Block 1 and 2 (0x60 and 0x61) are both Lifetime Data Block 1 (0x60)
- Lifetime Data Block 2 returns the data of Lifetime Data Block 3 with some errors. For example, I would like to read the Max Charge Current, Max Discharge Current, Max Avg Dsg Current and the Max Avg Dsg Power. I can not find these values in any Lifetime Data Block...

I tried reading with the EV2400 and it gives normal values. What is the difference between the EV2400 and the documentation?

It would be very nice if someone knows the answer to this.

Kind regards,
Lars Jansen