Hello,
I have attached my design, Where we connected MAX16009's output having sink current( 2mA)to LMZ12002 enable pin.
As i read from datasheet LMZ12002 it says it has internal pull-up resistor ,So when Vin comes LMZ12002 will be on if enable pin is not grounded(sinked).
My design needs to hold the EN pins of LMZ12002 to grounded by MAX16009 .
So my question is how much sink current needed to drive the enable pin of LMZ12002 "LOW".
Waiting for your feedback since my design is in crucial stage.
Regards,