This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Part Recommendations for Isolated Supply

Hi Team,

I have a customer that needs recommendations for an isolated supply with the following specs:

- Isolated 1/4W supply
- Input voltage (from battery): 3V-4.2V
- Output voltage: 3V-12V
- Max Current: 250mA
- Also required to be efficient when in sleep mode/light load

Please give me the top two suggestions we can offer them.

Thanks,
Michael Arriete