Other Parts Discussed in Thread: TPS2492
Greetings,
I have a TPS2492 set up with an overcurrent point of 50A.
When a load of >50A is applied, the gate voltage reduces, the fault timer ramps, and the MOSFET is turned off with out any damage.
If the overcurrent threshold is approached slowly, there is load point of about 49.5A to 50A where the FET gate voltage begins to reduce, however the timer does not start to run. If this current is maintained for an extended period of time, the result is violating the SOA of the FET (indefinite time spent in linear region). My power limit is set to 200W at Vprog, Since the Rdson of the FET is 1.5mohms, running at 49A is not near the Plim set by the voltage divider, so I'm confused why constant power engine begins lowering the gate voltage prior to the overcurrent being recognized and initiating the timer that is meant to protect the FET. I have verified this by sitting at 49A for extended periods of time with no issues.
Am I overlooking any features that would cause the constant power engine to lower gate voltage just prior to the overcurrent condition being recognized?
Thank you for your help.
Troy