This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost converter that has zero duty operation and forced PWM mode

Other Parts Discussed in Thread: TPS61253A, TPS61030, TPS61089, TPS61230

Hi,

Now our customer is looking for the boost converter that has zero duty operation and forced PWM mode. I have found TPS6123x and TPS61253x which have zero duty operation but don't have forced PWM mode. Do you have such converter which can meet following requirement?

  • Vin = 3.0V to 4.2V (Li-Ion 1 cell) and 5.0V (VBUS), switch input source
  • Vout = 5.0V
  • Iout(max) = 1.0A

Best Regards,

Sonoki / Japan Disty