Hi,
When using a non-isolated DC/DC converter,input and output capacitor are very important for the device operate correctly.
In tihs case,what parameters must we care?How to get the capacitor value in certain condition?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When using a non-isolated DC/DC converter,input and output capacitor are very important for the device operate correctly.
In tihs case,what parameters must we care?How to get the capacitor value in certain condition?
Thanks!
Hi John,
Thanks for your suggestion.I want to use TPS54160 for the design.The input is 36V,the expected output is 5V/1A.
How to choose the input and output capacitor correctly?Would you please offer more details for me?
For input capacitance see the datasheet section 9.2.2.5. TPS54160 requires at least 3 uF effective input bypass capacitance. it should be X5R or X7R. You have to take DC bias into account. 2 x 2.2 uF or 1 x 4.7 should be sufficient if the voltage rating is high enough. If your circuit is located a long way from your input voltage source or if a long cable is used , you may need some bulk electrolytic as well. The value is not critical, 47 or 100 uF is what I typically use.
For the output, see section 9.2.2.3. The transient requirement is usually the most stringent. I typically do not design with less than 22 uF of output capacitance. I am usually more conservative and use 2 x 22 uF or more. The reference circuit uses 47 uF, That is probably a good choice for many applications.
Alternately, you can use the online Webench tool to create your design. Webench tends to pick lower values of output capacitance than I prefer, but you can always change that within Webench.
Hi John,
If no input capacitor,what will happen when using the DC/DC converter?
Terry,
For the Boost converter, input capacitance is not so critical, but the output capacictance is very critical, put it as near to the IC as possible.
For the BUCK converter, input capacitor is very very critical, put it as near to the IC's Vin pin as possible, output cap is not so critical.
But both input and output need to put certain ammount of capacitors based on the output power and output ripple requirement. Or there will be stability issue or even can't startup.
BR,Helen