I noticed while modifying something else with a heat gun nearby, the output from my LM3429 was dipping/increasing unexpectedly. After messing around a bit I noticed that waving the heat gun over the dimming part of the PCB from about 5 inches away caused this behaviour to occur. I also noticed that this would happen if I applied pressure to the top of Q2 with a pair of tweezers. I noticed waving a soldering iron around Q2 that having heat at one side will brighten the output, and the other side will dim it.
I don't understand why this would be happening, especially since it was the part recommended in the datasheet and it's for LED driving which will generate heat.
Schematic and layout are below.
Q2: BC856BDW1T1G
U5: LM4120IM5-5.0