This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM46002 question about negative output

Genius 3900 points
Other Parts Discussed in Thread: LM46002

Hi, 

we are using LM46002 to generate  -5V from Vin=14~19V, and I am looking at this reference . could you please help on some questions as following ? Thanks a lot!

(1) It is concerned that will LM46002 still capable of 2A output current with -5V Vout? If not, what is the maxim Iout? We need about 1~1.5A max.

(2) I think LM46002 will refer to Vout(-5V) rather than GND(0V) in this situation. If so, all the "0V" voltage in datasheet shall be interpreted as -5V ?

for example, the Enable pin voltage threshold in normal buck mode is 1.2V and 0.4V, which will change to -3.8V and -4.6V. is this correct?

(3) Enable pin: as I analyze in (2),  if I use an MCU(LVCOM 3.3V IO port) to control EN pin, there shall be level shift circuits to satisfy the enable pin threshold. is there any recommendation?

(4) PowerGood pin : this pin will also need some interfacing circuit before connected to MCU. rigth?

(5) Sync pin: as for AC coupling, there is no need to do level shift. right?

(6) Bootstrap cap: the datasheet page 22 suggests 0.47uF but the reference design uses 0.1uF , what's the difference?