Hi Sir
we have do OCP test in TLV62085 EVB, but when we Vin 3.3V, Vout 1.2V the output current increase to 3.2A, then EVB will OCP.
but when i short power supply and EVB line distance. then out current will reach to 3.6A. or i add C5 capacitor value. then OCP also can reach 3.7A.
May you have advise me some suggestion? Due to DS is show the OCP should be around 3.7~4.x A
Bogey