Hi,
We're currently using TPS25942A with 9V to 15V input voltage and current limit around 3A.
TPS25942A behavior is to limit current to set level and eventually turn-off due to thermal protection.
We wish an e-fuse with this same behavior (current limiter) but that can withstand more time before turning-off due to thermal protection.
I've found the TPS24851. How does it compare to TPS25942A in terms of time it withstand in current limiting mode?
If necessary, please use this standard situation for comparison: input voltage of 12V, current limited at 3.0A, output voltage of 5.0V.
Do you need any additional information?
Do you have any other device suggestion? Maybe a controller? (reverse current blocking is a desired feature)
Thanks.