This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43000 as a variable output buck/boost converter.

Other Parts Discussed in Thread: TPS43000

Hi,

1) I'm planning to build a buck/boost converter using the TPS43000 with the specifications as below:


Vin: 2.5V-5V

Iout: <15A

Vout: 0-8V

2) is it possible to also be able to control the output voltage when using the TPS43000? Using voltage dividers on the FB pin creates a fixed output, is it possible for variable output?

Please help, thank you!