This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[BQ27541-200]read 0x2f of StateofHealth , it is alway "0"

Other Parts Discussed in Thread: BQ27541

     Currently I am working on BQ27541 gauge, , I need to SOH value for battery health feature.

 

I had flashed the golden image file into bq27541-200 ,  reset , enable "IT"

Then I  charge (to 4.2V)& discharge(to 3.5V) battery twice.

but after these steps

When I read 0x2f which is the SOH Status:, the value of that register is still 0x0.

0x0 means ”  0x00: SOH not valid (initialization)”

   Does that mean I still have to do something to activate SOH?