Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The LMZ31506 INH pin has an internal pullup current source, allowing the user to float the INH pin for enabling the device. The pull-up voltage level is approximately 2.8V when this pin is floating. There is no internal resistor divider on this pin.
Thank you for the answer. I'll give a reply it to my customer.
But I have a question. The result of LTspice was 8.5V, can I think it is wrong?
Best regards,
Yokota
I'm sorry to add a question.
If the INH terminal is 2.8V, I think it needs zener diode etc attached document(TPS625261 datasheet).
So if the INH terminal direct connection to the EN pin of the internal controller, I think it's voltage level isn't 2.8V.
What is correct?
Best regards,
Yokota