This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: Trouble chargin Vstor capacitor

Other Parts Discussed in Thread: BQ25504

Hello,
I am using BQ25504 with an input of 0,88V and 0,4mA. 
However Chvr input capacitor limits input voltage to 330mV. I supposed this was done in order to charge Vstor capacitor using cold start, however the capacitor charges very slowly until it reaches 330mV and then it discharges.  The UV_voltage and OV_voltage are in correct range according to the datasheet. Is it normal to limit the input voltage in such way? 

Thanks in advance!!