Hello Team,
I'm working on a design where I believe it will be Hotswap then ORing. I'm looking at using the TPS24742 in this design, but I need help selecting the proper MOSFET for my application. Does anyone have a recommendation?
I looked at the CSD17573Q5B and I'm using the design calculator for the TPS24742 to see if I might have any design issues.
Originally I had the CSD16415Q5, but it has a low gate to source voltage of 16/-12. I want something with 20V so the gate charge pump can't damage the FET. My output is 12V @ 20A.
I really appreciate the help!
Best Regards,
Ben