Other Parts Discussed in Thread: LM7171, CSD, CSD18542KCS, TIPD102, CSD16556Q5B
Hi,
I am designing a programmable dc electronic load circuit, with rating 0.9-3.3V and 0-30A current sink capability. I have referred to many circuits online which showed me simple op-amp with its output given to the gate of power mosfet.
Working of this circuit is as: say 100mV is given at the positive terminal of the opamp, the circuit working totally fine in simulation to give me 100/5=20A sinking through the mosfet. Opamp used: LM7171, Mosfet Used: CSD 18542KCS from TI.
I have made a board, and my circuit, though working absolutely fine in simulation, not working on board.
Following are the observations that I made:
a) output of the opamp should get modified depending on the voltage at the non inverting terminal of LM7171, however, its constantly giving 10V at the output even if voltage at non inverting terminal is 0. So, I believe feedback not working.
b) CSD18542KCS is expected to give nearly more than 100A when subjected to Vgs=10V, and Vds=0.1V, but its giving only 2A.
c) Even when there is more positive voltage at inverting terminal than nono inverting, output doesn't go negative.
Any suggestions would be welcome.
Thanks in advance.