Dear All,
I'm Designing a system supplied by a solar panel (Vmp 6.5V) and a Battery Li-ion (4.2V). I would like to use the bq24650 as a power path.
I have a couple of questions about the bq24650EVM:
1-) To set the VOUT of the EVM (Battery Voltage) , is neccesary to program it via R13 and R15 . But how do I configure the VSYS voltage to provide 5V?
2-) If there is not enought solar irradiance in the panel to supply the the VSYS. What are the conditions to start the battery as a main power supply throught VSYS pin with 5V?
3-) Is it possible to connect parallel cell batteries for charging trought this IC?
Looking forward to your kind reply.
Regards,
Juan Gaines