hi
i have one 5.7" TFT lcd. In which LED's arangement in a backlight is as shown in an attached file.i am looking for it's driver.i zeroed down on TPS61041 & TPS61161
1. TPS61041 if i put RS=8.1 ohm (1.230 v / 150ma backlight max current limit is upto 210 ma.) across FB pin
2 TPS61161 if i put Rset=1.5 ohm (200 mv / 133ma backlight max current limit is upto 210 ma) across FB pin
Will it work for my BACKLIGHT i am confused because they are for series LEDS & my backlight have 3 series leds in 7 parallel rows.my backlight connector has 2 pins only as shown in attached file. If not someone give me some suggestions which led driver i should use. I want to use PWM method only not analog method for dimming.waiting for your reply.