This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Communicating to a bq2083

Other Parts Discussed in Thread: BQ2083-V1P3, EV2400, BQ2083

Hi,

I'm attempting to communicate to a bq2083-V1P3 fuel gauge. 

I have installed bq2083-bq2085 EVSW Install v2p5 and am using a EV2300 on a Windows XP machine. The SCL/SDA lines on the battery are pulled up to 3.3V. The software does not display any telemetry; it states "Target Board Not Responding". I have also tested communication when using a EV2400 and an EV2200. 

I've confirmed that the fuel gauge is powered (3.3V provided from AFE) and have also confirmed that the fuel gauge is operating (CLKOUT from FG is a clean 32khz square wave). I have confirmed the fuel gauge is not held in reset (MRST is low). 

I have not achieved successful communication with this fuel gauge. What other elements should I be investigating or using?

Lucas