This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24073 - BATT to OUT maximum peak current?

Other Parts Discussed in Thread: BQ24073

In the BQ24073 datasheet the maximum output current Io (continuous) is specified at 5A in BATT discharge mode.  

When you work backwards with an RDSon of 100mR it doesn't take long to work out why.  However is there a maximum for a peak transient current ?

I have a LED driver that will draw up to 6.5A peak for approximately 200ns which then falls to 3A peak within a millisecond (5 cycles).   Will this high peak current damage the wirebonds within the BQ24073 ?

Thanks for looking...