We have an application that seems to be right in-between the specs of the 65130 and 65131. As stated in the subject we'll have a 5V input (coming from USB) and will be generating +/-12V outputs. Our peak current draws might be up to 150mA. There are plenty of load graphs in the datasheet but they don't quite show our conditions for the 65130.
Does anyone happen to have any data that would show if we would be OK with the 65130 and can save a little money? Availability isn't great on these parts so we wanted to place an order while we finished our design. The good news is that both parts seem to be drop in replacements so one design will handle either part.
Any feedback would be appreciated.
Thanks,
George