This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013BEVM-764 WPC 1.1 Compatible Fully Integrated Wireless Power Receiver IC Evaluation Module and bq500412EVM-584 evaluation module

Other Parts Discussed in Thread: BQ51013BEVM-764, BQ500412EVM-584

Question 1: I want to buy the BQ51013BEVM-764  and  bq500412EVM-584 evaluation module. I don't know whether they can match together and work together.

Question 2: Does the BQ51013BEVM-764 receiver have coil inside it? I didn't see any coil shown in the picture .http://www.ti.com/tool/BQ51013BEVM-764.    Do I need to buy a coil to attach to it?

  • Fan,

    Yes, the bq51013BEVM-764 will work well with the bq500412EVM-584.  Any of TI transmitters will work with any of the TI receivers.

    Yes, the bq51013BEVM-764 does come with a coil.  The Bill of Materials in the User Guide shows 3 coil options that may be on the EVM.

    The coil is attached to base of the poly case.  There is space between the coil and the EVM board to allow you to put other electronics that may be in your final solution - including a battery.

    It is also possible for you to choose you own coil and replace the one that comes with the EVM.  If you do replace the coil, see section 9.2.1.2.2 on capacitor modifications that may be required for the new coil.

    Regards,

    Dick