This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100-G1 State Of Health configuration/calculation

Hi,

since we want to tell the user when the lead acid batteries should be exchanged we rely on a good state of health value.

SLUSBZ5A says:

8.3.2.10 StateOfHealth(): 0x2E/0x2F
This read-only command pair returns an unsigned integer value, expressed as a percentage of the ratio of
predicted FCC (25°C, SOH current rate) over the DesignCapacity(). The FCC (25°C, SOH current rate) is the
calculated full charge capacity at 25°C and the SOH current rate that is specified in the data flash (State of
Health Load). The range of the returned SOH percentage is 0x00 to 0x64, indicating 0% to 100%,
correspondingly.

So it depends additionally on the SOH Load (Dataflash: SOH Load I Min: –32767 Max: 0 Default: –400 mA).

What does this parameter actually mean? Is it the average estimated/expected current load during discharge?

Sebastian