This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beagle bone black turned OFF when running on battery

Dear All,

We are working on a custom board based on beagle bone black + TPS65217C where TI-SDK-8 is running. We had some application running on that what's happening is when we are running on battery, board is getting shut down, even though battery has enough voltage. It's not happening every time, If we start running for overnight after 6+ hours it is getting shutdown. Can you please suggest us why it is shutting down? How can we debug this issue?


When the board is running on battery it will go to sleep mode and immediately wakes up due to wake up source.
So briefly 6 seconds it will be in normal mode and after that it will enter into deep sleep mode and after around 6 seconds it will wake up due to wake up source. So it will be keep on happens like that.

After around some definite hours board is shutting down.

Please help us to debug.

Thank you,