This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28089

Other Parts Discussed in Thread: UCC28089, LM5039

Dear team,

My customer would like to have the followings informations:

I would like to have information about one of your products, which is the UCC28089 component.

This component is for a given op Tj max 150 ° C, but with Tamb and TJOP recommended to 105 ° C.

This seems surprising that Tamb and TJOP is the same. Is it normal ?

The problem I have is this: the room temperature is lower than 105 ° C, but with self-heating of the component, it will probably be closer to 110 ° C.

This component, although ASSETS seems relatively old (the datasheet was in 2006).

Otherwise, would you have an oscillator frequency component with programmable dead time and to offer the following features:

- Vin = 15V nominal (the UCC28089 is advised that up to 14 V. It is therefore lower the voltage).

- Oscillator frequency: 100 to 800 kHz

- Timeout: 100 to 1 s - Temp: [-40: +125 ° C] Tj

- Soft Start

- No need necessarily to FB, the goal is to have the component most simple and compact.

Do you have any alternative solution ?

Thanks for your support, Maxime