This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65263-Q1 / Efficiency

Guru 20090 points
Other Parts Discussed in Thread: TPS65263-Q1

Hello,

Could you please let me know the efficiency of TPS65263-Q1 on the following conditions?

All input voltage is 8.7V
Lower switching frequency 200kHz is acceptable.

<Condition 1>
BUCK1: 5V, Iout=70mA
BUCK2: 5V, Iout=280mA
BUCK3: 5V, Iout=255mA

<Condition 2>
BUCK1: 5V, Iout=100mA
BUCK2: 5V, Iout=890mA
BUCK3: 5V, Iout=370mA

<Condition 3>
BUCK1: 1.2V, Iout=395mA
BUCK2: 2.5V, Iout=98mA
BUCK3: 3.3V, Iout=257mA

<Condition 4>
BUCK1: 1.2V, Iout=545mA
BUCK2: 2.5V, Iout=149mA
BUCK3: 3.3V, Iout=371mA

<Condition 5>
BUCK1: 1.2V, Iout=700mA
BUCK2: 2.5V, Iout=108mA
BUCK3: 3.3V, Iout=257mA

<Condition 6>
BUCK1: 1.2V, Iout=1000mA
BUCK2: 2.5V, Iout=297mA
BUCK3: 3.3V, Iout=718mA

Best Regards,
Ryuji Asaka