Hi
Could you tell me about TPS92513 inducter?
My customer use TPS92513 the following condition.
・Vin=24V
・Vout=14.5V
・Iout=380mA(typ)/600mA(max)
・Fsw=1MHz
・LED ripple current target : under 10mA
Customer would like to use 100uH inductor above condition.
Is it possible to use 100uH above condition, and please give me recommend value of the inductor and capacitance?
If you have concern point, please tell me.
Best Regards,
Yusuke