This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100-g1 terms

Other Parts Discussed in Thread: BQ34Z100-G1, BQ27510, BQSTUDIO

Hello

 

My customer have several questions  about terms and also usage of BQ34z100-G1.

Would you please let me know?

 

Q1  RFACTSTEP

RFACTSTEP : We see RFACTSTEP is used to enable resistance update range set by Min/Max Res Factor.

Also,if RFACTSTEP =0, there are no limitation for Res Factor update....

What is the benefit of RFACTSTEP= 1 ?

What is the actual case customer set this to 1?  Please let us know the usage.

 

Q2 QPCCLEAR

I had answer from local FAE  that  "QPCCLEAR : Default=0, Allows the gauge to reset the Passed Charge that has accumulated

during rest, when discharge starts."

However, what is the actual case that customer should  set QPCCLEAR to =1 ?

We want to know the usage.

 

Q3 Temp Hys

The usage of Temp hys in bq34z100-g1 is same as BQ27510/BQ27520 case?

We see BQ27520_G4 TRM  note ( sluua35 )wrote " [Chg Inhibit Temp Low + Temp  Hys, Chg Inhibit Temp High–Temp Hys] ".

 

 

Q4  Cycle Count

We see two  " Cycle Count" in bqStudio.

One is "Configuration" tab, and  other is in Gas Gauging tab.

User should setCycle Count  in the Configulation tab? 

Which is the Cycle Count in the Configulation tab in 0x2C/0x2D?) 

 

Q5  Max Error()

Max Error() : It seems Read only register,but what does this indicate in the the operation in Gas Gaugeing?

I could not understand well in the Table4 page 15 of data sheet.

What is the usage( benefit ) for customer?

 

Q6  RNSN1,RSNS2,IWAKE

Vth is same '+5mV or -5mV'  in case 1,0,1 and 1,1,0.

However  what is the difference 1,0,1 and 1,1,0 for another function?   Every thig is same?

 

Q7  BAT resister dividerI

Customer had better use OP amp for BAT pin,,   isn't  it?

In the app note slua760 shows the second resister 16.5Kohm. But input resistance Zadc is 100Kohm as per datasheet.

Why is the recommendation is between 15K to 25Kohm for second reisiter because input resistance is 100Kohm?

 

I am sorry such a basic questions..

Best Regards