PMIC Team,
I am working of an OMAP3530 design for a customer and I have a couple of questions on the TPS65930 PMIC:
1) For USB we plan to implement a USB device only, no OTG and no host. How should I handle the VBUS, ID, and VPRECH pins?
2) I need a rail to power a thermistor (<1mA) connected to ADCIN0. The datasheet says that VINTANA1 (ADCIN0’s rail) is capable of 50mA but is for internal use only. Should I take that literally, i.e. use a different rail (e.g. VDAC_OUT or VAUX2_OUT) to power my thermistor circuit?
3) Do I really GND the PreDriv_R output if I am not using it?
Thanks,
Brad Nielsen 425.444.7083