Hi
I have two question about thermal shutdown.
1.How much is the variation of thermal shutdown and thermal swing shutdown threshold? (On the datasheet, there is only typical value)
2. Regarding thermal shutdown and thermal swing,
- When T(fet) > T(sd) , the respective output turns off. That means that the only channel which is over T(sd) turns off. Is that correct?
- When T(logic) > T(sd), the all channel turns off. Is that correct?
- When T(fet)-T(logic) > T(sw), the only channel which is T(fet)-T(logic) > T(sw). Is that correct?
Regards,
Koji Hamamoto