have a question about TPS54541:
In case of the condition Vin < Vout, does this device support reverse current protection
- when it is powered and switched off via it's EN-Pin?
- when Vin = 0V, and Vout is up to 5V?
Regards, Niels
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello John,
thank you for your fast answer.
Do you have a suggestion to add reverse current protection to the TPS54541?
Regards, Niels
Hello John,
the source of the pre-bias voltage on the output is another power-supply that may also power the board.
Regards, Niels