Hi L&S team,
Our customer has some concern about the TPS709, would you kindly help look into this?
The TPS709 devices are stable with output capacitors with an effective capacitance of 2.0 μF or greater for output voltages below 1.5 V. For output voltages equal or greater than 1.5 V, the minimum effective capacitance for stability is 1.5 µF. The maximum capacitance for stability is 47 µF. The equivalent series resistance (ESR) of the output capacitor must be between 0 Ω and 0.2 Ω for stability.
1. Could you kindly show me the transfer formula of the feedback loop inside the LDO?
2. What's the minimum Cout for stability?
Best regards,
Bell