In the TIDA 0049 reference design (10S 50A toolpacks design) there is a TVS fitted between both pack + and - and load + and -.
Is there a need for the TVS? For our application, an extra wire will need to be installed to bring the top cell connection to the BMS with low impedance (other than the sense wire).
Interrupting current by stopping discharge will certainly create a voltage spike, depending on the switch speed of the mosfet - and the discharge current being interrupted. Can the TVS be moved to Drain-Source of the Mosfet instead of Pack + and -?
Looking for input on this issue, than you in advance.