I just bought a LM2623EV evaluation module. The input was connected to a DC PSU at 3 V. I measured the output using a DMM and expected to see 5 V.
When I turned on the PSU, it showed that the module was drawing 1 A. I did not place any load (resistor) across the output. Even when I placed a large resistor (56 kOhm), it still drew 1 A.
I did continuity test on the pads and could not find any short to ground.
Note that: the DC PSU is working and is not at fault. I did not modify the board. I tested it out-of-the-box.
Any idea why it was behaving this way?