This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bootstrap diode ratings LM5106

Other Parts Discussed in Thread: LM5106, LM5109B

Hi all,

I am trying to select the bootstrap components (capacitor and diode), to be used with the gate driver LM5106 (for a synchronous buck or boost application).

I am using the N- MOSFET IPP075N15N3 G, whose total gate charge (max value) is 93C. I suppose that is the charge I need to supply to the gate to turn the mosfet on.

I would like to select the bootstrap diode.

- Bootstrap diode voltage rating: same as DC bus voltage rating (e.g. 100V)

- Bootstrap diode current rating If? Is it correct to use If=Qg*fsw, where Qg is the total gate charge and fsw is the converter switching frequency (e.g.) 200kHz, so in this case If = 0.0186A? 

It looks like a rather small current rating value, I wanted to make sure it is correct.

Also, is it safe NOT to use a boot resistor in series with the bootstrap diode? Or do I have to include a boot resistor in series with the boot diode in my circuit? If so how do I choose the boot resistor?

Thanks a lot,

Leonardo