Since in our design only a few parts are testable with a passive ICT, we have to define a functional test. Is there a chance to test an assembled PCB without connecting a receiver coil and using a wireless transmitter device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Burkhard,
What sort of testing do you need to do on the bq51013B circuitry?
If you are interested in testing the circuitry to be powered by the bq51013B, you can apply 5V to OUT. The would be no issues with the bq51013B.
If you want to test the bq51013B, you could consider putting a sine wave on the AC1/AC2 pins similar to what would occur with the RX coil on the Transmitter. A simple function generator may not have enough power to get what you're looking for, this may need to be amplified.
Since the typical "ping" frequency is 175kHz, that is a safe place to start.
Regards,
Dick
Burkhard,
Thank you for the details. The only way to test the full values is to run on a TX. When you force AC1/AC2, that prevents the communication back to the TX so the COMMx capacitors cannot be tested. The CLAMP capacitors are mainly for protection so hopefully you don't test those. The BOOT will be tested if the OUT turns on. RILIM can certainly be tested as you note. TS/CTRL depends on how you are using it. Is it a thermister circuit or simply the 10k resistor?
As I noted on the original response, the signal you put on AC1/AC2 must be able to supply the required current.
Efficiency will need to be relative. TX+RX system, the communication from the RX sets the frequency to the optimum level for best efficiency. If you force a frequency, you may not be at the best value. In normal operation, the Rectifier voltage (seen at the RECT pin) is the key to efficiency. At light loads (as seen in datasheet plots) the efficiency is not as important as maintaining the ability to respond to load steps so RECT is higher than it needs to be for optimum efficiency. At heavy loads, the communication sets the RECT voltage as close to OUT as possible to maintain the lowest loss in the RX.
Regards,
Dick