This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2420 Imon output samplig with ADC - is buffer needed?

Other Parts Discussed in Thread: TPS2420

Hello,

I'd like to use TPS2420 as output of 12VDC with max 1A. Datasheet contains table with values of all passive components to achieve that. My question/problem is related to Imon. It will be about 15uA (Imon=Iout/66k) for Iout=1A.To produce 2.5V output I need Rmon=158k. Do I need opamp buffer and antialiasing filter to sample Imon with 10-bit MCU ADC at 400Hz maximum? I assume that Imon changes as fast as Iout and is not averaging so with dynamic load generating spikes, dips etc. some LPF would be useful, wouldn't it?

Could you suggest a circuit to glue these things together?