This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118-Q1 / CISPR25 class3

Guru 29720 points
Other Parts Discussed in Thread: LM25118-Q1, LM25118

Hi Team,

My customer is looking for the automotive buck-boost device that meets the following requirement.
---------------------------------
Vin: 5-40V
Vout: 12V
Iout: 4A
---------------------------------
I believe LM25118-Q1 is appropriate device that meets the requirement above.
However he also would like to pass CISPR25 class3 in his application.

Is it possible to achieve it with LM25118-Q1?
Is there any data or reference design with LM25118-Q1?

Best Regards,
Yaita / Japan disty