A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS65185Hello, all.
I want to know lot number of the TPS65185.
It has text below on surface of the chip I have.
E INK
TPS65185
TI 38I
APFX G4(with underbar)
best regards,
Hi Tomo,
I am trying to get more information regarding your request from the team. Please let me know why is the lot number needed? Do you have any failure?
Yes, I have a problem.
The TPS65185 did not output the VEE voltage properly.
I expect -20V output, but -15.8V only is output.
VEE_FB pin voltage is -0.786V.
VEE_DRV pin seems to not properly work.
VEE_IN voltage is -16.12V.
Other output is good.
I made 4pcs PCB boards that installed TPS65185 in first of the year.
4pcs board were properly work.
Recently, I made 2pcs PCB boards again. GERBER, BOM and PCB Vendor are same.
But problem occurred in 2pcs boards. Problem is same.
I checked my schematics and board, but I did not find any strangeness.
So I want to know whether this problem are related with the lot number.
Personally, i don't think this is an issue with process. The chances of 2 parts having quality issues out of 6 is extremely rare. I would double check the board for manufacturing defects before we proceed this route.
Also, can you please send me a email to jayanth_kruttiventi@ti.com. If needed, I will connect you with our quality team and they can better help you in this regard.
Thank you for your reply.
I had to shipping out the custom board in the end of last month, so I was replaced to new TPS65185 and checked behavior.
After replaced, our custom board worked fine.
I thought it might destroyed at reflow.
I wanted to know how to check lot number at minimum, but I need no more answer, because I was replaced the chip to clear a problem and I was dispose of chip that has problem.