Hi,
My customer has question about LM3464.
Could you tell me about questoin?
[Question]
My customer considers to use LM3464 under the following condition.
Vrail(nom)=28V *Boost convertor output
Vf=30V
Iled=2A/ch
LED=two Strings
- Can the device be set two strings configuration?
- How much is the maximum current per channel?
Does it depend on power dissipation of external FET?
- My customer wants to use boost convertor for the primary power supply.
e.g. LM5122
Can the device use boost convertor for the primary power supply?
- My customer wants to use the stabilized power source equipment for primary power supply on simple evaluation.
Can the device use the stabilized power source equipment for primary power supply?
Best Regards,
tateo