Hi,
My customer has question about TPS61043.
Could you tell me about questoin?
[Question]
- My customer considers to use TPS61043 for 2cell application.
So my customer consider the design separating Vin from power stage.
Can TPS61043 be used with higher input voltage as long as the control circuitry is kept separate from the power stage?
Please see figure below.
- How is the condition of soft-start function is enabled?
Is it only when device is start-up or every time PWM High signal is inputted for CTRL pin?
My customer is concerned about rush current.
Is there waveform of LED current at rising edge of PWM signal?
- Pulling the CTRL pin to GND for more than 32 ms or 10 ms disables the device.
What is the difference between 32 ms and 10 ms?
Does 10 ms be accepted only at Duty cycle below 1%?
Best Regards,
tateo