This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestion for a buck converter

Other Parts Discussed in Thread: TPS62125, TPS62140A, TPS62160

Hello,

I need to design a dc dc converter and my specifications are

Vin(min) = 10V

Vin(max) = 15V

Vout = 5.5V

Iout = 0.2A

When I enter these Parameters into search table of TI , i get 100's of converters and donot understand how to choose from.

Can someone tell me which Parameters I can further look into to narrow my selection and also suggest some commonly used buck converters for my specifications.

Thanking you

Spanika Kamuni